検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

Long Term Evolution:LTEテスト

ご覧になるためには、ブラウザのJavascriptを有効にしてください。また、Adobe Flash Player が必要です。

Flash ダウンロード 

KeysightのLTEデザイン/テスト製品のラインナップ - 詳細な解析、高い信頼性

 

Keysightの製品を使用すれば、LTEデザインの「より詳細な解析」が可能です。Keysightは、デザインの不確かさの低減、高性能LTE製品の開発の高速化/簡素化、原因究明の迅速化を実現します。業界初のLTE-Advanced用テスト・ソリューションもご用意しました

LTE テクノロジーの詳細:LTEテクノロジーの概要

LTEに関するアプリケーション・ノート、CD、その他のリソースをご希望の場合:詳細

LTEの開発ステージに適合する製品をお探しの場合は、以下のリンクを参照してください。

YouTubeビデオを見る 

1-13 / 13

並べ替え
MIMO Over-The-Air Research, Development, and Testing 
International Journal of Antennas and Propagation, May 2012 article provides information on the many challenges of identifying the optimal channel models and test method(s), for MIMO

記事 2012-05-09

 
Two-Stage Over-the-Air (OTA) Test Method for LTE MIMO Device Performance Evaluation 
International Journal of Antennas and Propagation, February, 2012, article introduces a novel, flexible, and cost-effective method for measuring MIMO OTA using a two-stage approach.

記事 2012-03-28

 
LTE-Advanced…Already? 
Article reprint from OSP magazine detailing the additional changes LTE-Advanced brings to the Network already working to implement 3GPP LTE.

記事 2011-09-01

PDF PDF 695 KB
The MIMO Antenna: Unseen, Unloved, Untested! 
Microwave Journal (August 2010) article (.pdf) written by Agilent’s Moray Rumney. With the shift of MIMO from theory to real world this article focuses on performance testing in real world conditions.

記事 2010-08-20

PDF PDF 693 KB
Measuring MIMO In LTE Tx And Rx Tests 
Find the right combination of LTE test instruments and techniques to evaluate the performance of Long Term Evolution (LTE) components and systems under real-world conditions. A link to the MWJ article by Agilent.

記事 2010-08-18

 
A primer on MIMO in LTE 
An article in Electronic Products, written by Agilent’s Jan Whitacre, exploring the special employment of multiple-input, multiple-output radios to utilize spectrum in Long Term Evolution (LTE) systems.

記事 2010-02-01

 
IMT-Advanced:第4 世代の無線通信が具体化 
いわゆる3.5G、3.75G、3.9G 規格の開発に加 えて、第4 世代(4G)に対する期待が高まっています。また、3GPPのワーキング・グループの会合に続いて、4G 無線通信に関するワークショップが、中国のシンセンで開催されました。

記事 2009-05-18

PDF PDF 961 KB
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

記事 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

記事 2009-04-09

 
Expert Advice: The Importance of Average vs. Peak Performance in Cellular Wireless 
The average efficiency of the cell remains much lower than the peaks. November 2008 article by Moray Rumney linked with permission by Microwave Journal.

記事 2008-11-17

 
Analyze Antenna Approaches for LTE Wireless Systems 
Multiple-antenna techniques are a large part of improved performance in LTE wireless systems, but they must be properly understood in order to be properly tested.

記事 2008-08-13

 
LTE ARQ and Re-segmentation 
Link to August 2008 Microwave Journal Article

記事 2008-08-08

 
3GPP LTE:SC-FDMA の概要 
この記事では、LTE が移動体通信のエコシステムに何をもたらそうとしているのかを取り上げています。

記事 2008-03-21

PDF PDF 2.86 MB