您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

是德科技無線連接技術

WiMAX • 是德科技 低功耗測試專家,物聯網 IoT • MIMO • Bluetooth • 802.11 WLAN • NFC / EMV 測試 • 超寬頻(UWB)測試 • ZigBee • 數位電視

即刻獲得前所未有的量測洞察力。您知道,從此之後您將與眾不同。是德科技獨有的硬體、軟體和專業人員組合,可為您提供前所未有的量測洞察力。我們的測試設備和設計軟體傳承超過 75 年的量測技術領先優勢,是您可完全信賴的得力助手。新興和現有無線技術正持續演進並創新,使得設計工程師在設計和測試各種建構互連世界的元件、模組和裝置時,面臨了全新的挑戰。是德科技是全球領先的電子量測大廠,具有產業領導地位,可提供橫跨整個技術週期的全系列測試和設計解決方案,從模擬、研發、設計驗證、先期認證測試、相符性測試、製造,一直到網路部署及服務保證,全都涵蓋在內。

是德科技積極參與無線技術標準的制訂,因此我們知道如何確保您的設計符合最新標準。我們可最先提供符合標準的無線測試和設計工具,涵蓋從 Bluetooth 到 60 GHz 802.11ad 等所有技術。我們堅持以未來為導向的儀器設計理念,讓您能從容因應不斷變化的技術,始終屹立在技術發展前端。利用從當前的研究和開發階段到未來的製造和部署階段一脈相承的量測技術,您的投資可發揮最大價值。我們的設計與測試工程師和專家可為您提供切實可行、卓越有成的建議和協助,大幅增強您在全球各地團隊的技術實力。我們還經常發佈有關物聯網5G蜂巢式通信MIMOWLAN 測試等方面的白皮書、應用指南和網上直播,即時為您提供最新的專業技術。

觀看YouTube影片 

1-12 / 12

排序:
Dual Channel MIMO Measurements for WiMAX™ Wave 2 
In WiMAX Wave 2 systems, a variety of dual-channel measurements can provide essential insight into their operation and performance. Article written by Ben Zarlingo and linked with permission from Wireless Design and Development.

專文 2009-06-26

 
New Solutions Put Wireless To The Test 
Recent advances have made it possible for test vendors to provide off-the-shelf chipset-specific solutions for Wi-Fi, Bluetooth, and WiMAX RF test. Linked with permission from Mobile Dev & design.

專文 2009-06-11

 
MIMO and the Battle Between LTE and WiMAX™ 
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

專文 2009-04-10

 
Test solutions soup up for 4G 
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

專文 2009-04-09

 
A Day in the Life of a Mobile WiMAX™ Handset 
April 2009 featured article in Microwave Products Digest

專文 2009-04-01

 
Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices 
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

專文 2009-01-11

PDF PDF 1.37 MB
What Every RF Engineer Should Know: OFDM & WiMax 
Feature story by Janine Love.

案例研究 2008-12-27

 
First Pass Accuracy with Momentum GX for WiMAX Design 
Archived article at Microwave Product Digest discussing the challenges for designers in meeting cost and power consumption goals, using 3D-Planar electromagnetic (EM) simulation technology.

專文 2007-11-01

 
Unraveling Modulation Quality in Mobile WiMAX™ Uplink and Downlink with Multiple Zones and Bursts 
An article written for Microwave Journal addressing the difficulty in ensuring that the modulation quality of the WiMAX radio is sufficient for optimum RF performance and that it will perform according to industry standards.

專文 2007-11-01

PDF PDF 762 KB
WiMAX™: Plotting A New Path To Global Broadband Mobility 
Archived article at Canadian Electronics identifying innovations in test and measurement to support the innovations in the industry.

專文 2007-09-01

 
Validating IEEE 802.16e Designs With The Mobile WiMAX MIMO Library 
The IEEE 802.16e standard, often referred to as mobile WiMAX, specifies air interfaces for broadband wireless access (BWA) systems.

專文 2007-05-08

PDF PDF 524 Bytes
WiMAX™: The Next Generation of Broadband Wireless Access 
Article reprint from Electronics in Canada. This article provides anoverview of the 802.16 standard, theWiMAX forum, and key applications.

專文 2004-09-01

PDF PDF 428 KB