这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

无线连通性

全新视野,可以瞬间拥有。而您立即知道,自己从此与众不同。是德科技依托独有的硬件、软件和人员组合,帮助您开启全新的测量视野。我们的测试设备和设计软件传承 75 年以上测量技术领先优势,是您可以信赖的可靠助手。新兴和现有的无线技术一直在持续不断地发展创新,这給设计人员设计和测试各种构建互联世界的元器件、模块和设备带来了新挑战。作为全球领先的电子测试测量公司,是德科技将继续站在这一领域的最前沿,提供跨越整个技术生命周期 ― 从仿真、研发、设计验证、预兼容性测试、一致性测试、制造到网络部署及服务保证 ― 的全系列测试和设计解决方案。

我们知道如何确保您的设计符合最新标准。作为负责定义技术标准的无线标准组织中最积极的成员,我们一直最先提供符合标准的无线测试和设计工具,范围覆盖从蓝牙到 60 GHz 802.11ad 的所有技术。我们坚持面向未来的仪器设计理念,使您可以更容易地适应不断变化的技术,始终屹立在技术的最前沿。利用从当前的研究和开发阶段到未来的制造和部署阶段一脉相承的测量技术,您的投资可以发挥最大的价值。我们的设计与测试工程师和专家可以为您提供切实可行、卓有成效的建议和协助,极大增强您在全球各地的团队的技术实力。我们还经常发布有关物联网5G蜂窝通信MIMOWLAN 测试等方面的白皮书、应用指南和网上直播,即时为您提供最新的专业技术。

观看 YouTube 视频 

1-10 / 10

排序:
MWJ Article: Eye on 802.11ax: What It Is and How to Overcome the Design & Test Challenges It Creates 
Wireless access to data has become an everyday necessity for both consumers and enterprises. In the last 30 years alone, unfettered access to information has transformed entire industries, fueling growth, productivity and profits.

文章 2016-05-20

 
What is the difference between IEEE 802.11ac and 802.11ad? 
Microwave & RF article, April 2013. The goal is for all IEEE 802.11 standards to be backward compatible and for 802.11ac and 802.11ad to be compatible at the medium-access-control (MAC) or data-link layer. They should differ only in physical-layer (PHY) characteristics. Read about how that goal is being attained.

文章 2013-04-23

 
Tackling MIMO Design and Test Challenges for 802.11ac WLAN 
This article from Microwave Journal shows how the system engineer can use system simulation to help understand the design performance and design requirements needed to achieve transmitter system-level metrics such as EVM.

文章 2012-03-11

 
802.11ac 无线局域网: 新技术及其对设计和测试的影响 
EE times article by Agilent’s Mirin Lew describing the 802.11ac, the technical challenges and comparisons to earlier technologies.

文章 2011-11-09

 
802.11ac Wireless LAN: what’s new and the impact on design and test 
EE times article by Agilent’s Mirin Lew describing the 802.11ac, the technical challenges and comparisons to earlier technologies.

文章 2011-11-09

 
802.11ac 无线局域网: 新技术及其对设计和测试的影响 
安捷伦科技公司的 Mirin Lew 在《电子工程专辑》的文章中介绍了 802.11ac、其技术上的挑战以及与先前技术的比较。

文章 2011-11-09

 
Caution: MIMO Test Challenges Ahead 
Article published by Wireless Design & Development on MIMO testing challenges and methods to achieve higher data rates such as two0 and four-channel MIMO.

文章 2010-09-20

PDF PDF 70 KB
注意: MIMO 测试当前面临的挑战 
该文章由《无线设计和开发》发表,介绍了 MIMO 测试的挑战,以及获得更高数据速率的方法(例如 2 通道和 4 通道 MIMO)。

文章 2010-09-20

PDF PDF 70 KB
WLAN promises mobility in this fast-paced world 
The residential market is the fastest growing segment of the wireless LAN business.

专访 2003-09-01

PDF PDF 253 KB
A WLAN Test System using Test Equipment with EDA Software 
This Article by Dingqing Lu & Jinbiao Xu details a test system configured from basic h/w test equipment: signal generator, vector signal analyzer connected with EDA software for testing WLAN systems.

文章 2003-05-01

PDF PDF 264 KB