Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

MIMO Test

A challenging antenna technology, MIMO (Multiple Input, Multiple Output) is improving spectral efficiency (bit/sec/Hz), signal quality and cell coverage. MIMO is being used in multiple technologies including LTE-Advanced, WLAN and now being heavily investigated for new 5G technologies. Being a complex technology and an evolving standard for multiple technologies, MIMO provides hidden roadblocks and requires its own suite of measurements. Keysight's solutions are ready to enable deeper insights, especially as the standard evolves. In design and test, Keysight's solutions support innovation across new and existing technologies and allows engineers to transform ideas into reality.

MIMO Test Insights

Keysight RF and Digital Learning Center - A commitment to learning with industry experts

Explorer les vidéos YouTube 

Affiner la liste

retirer tout le raffinement

Par industrie/technologie

Par type de contenu

1-6 sur 6

Tri:
Introduction of LTE-Advanced Signal Generation and Analysis at Mobile World Congress March 2011 
Keysight’s European Marketing Manager, Renaud Duverne, introduces new capabilities capabilities such as carrier aggregation and answers questions about LTE-A early adoption, reducing the cost of test, transformative technologies and the challenges of growing video traffic.

Démonstration de base 2011-03-14

 
Demonstration of analysis of un-impaired and impaired WiMAX(TM) MIMO signal  
This video contains an analysis of a 2x2 WiMAX MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an un-impaired signal and signal impaired by pedestrian fading are examined.

Démonstration de base 2011-03-02

 
Demonstration of analysis of an un-impaired MIMO WiFi signal 
This video demonstrates how Keysight’s N7100 Multichannel signal analysis platform can identify and troubleshoot problems in a WiFi signal.

Démonstration de base 2011-02-22

 
Demonstration of analysis of un-impaired and impaired LTE MIMO signal 
This video contains an analysis of a 2x2 LTE MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an unimpaired signal and signal impaired by static fading are examined.

Démonstration de base 2011-02-22

 
N7100 Multi-channel Signal Analysis support of MIMO development 
The N7100 Multi-channel analysis platform helps solve difficult problems in MIMO development. The video is an overview of the many measurement and analysis capabilities of the N7100.

Démonstration de base 2011-02-22

 
LTE MIMO Composite EVM  
This is a demonstration of a 2x2 LTE MIMO system configuration where the Keysight 89600 VSA software and Keysight N9020A MXA signal analyzers are used to make an LTE MIMO composite EVM measurement on signals from the Keysight N5182A MXG signal generators.

Démonstration de base 2011-01-12