이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

RF 및 마이크로웨이브

1-25 / 103

정렬방식:
How to Estimate Voltage Spikes from Layout Parasitic Inductance in Switched-Mode Power Supplies 
We showed you how to deal with layout parasitic inductance in our previous video entitled “How to design DC-to-DC power converters”, but a frequently asked question was “When should I start to worry about layout parasitics inductance? Is there a quick rule of thumb that says kind of ‘Caution: Further investigation’s needed?’” The answer is yes and this follow up video is about how to make these estimates.

사용방법 동영상 2017-07-17

 
EDAcafé - DAC 2017 Interview: Michel Azarian, Silicon RFIC EDA Program Manager 
Sanjay Gangal from EDAcafé interviews Michel Azarian (Keysight Technologies' Silicon RFIC EDA Program Manager) at Design Automation Conference (DAC) 2017.

기본 데모 2017-06-22

 
IMS 2017: What's new with Keysight's SystemVue 2017 
Keysight's How-Siang Yap demonstrates the new features of SystemVue 2017 for Microwave Journal at IMS 2017 in Hawaii.

기본 데모 2017-06-21

 
IMS 2017: Top 5 Must-See 5G Products 
Sponsored by Qorvo, Wireless Design and Development (WDD) counts down the best 5G products out of this year's International Microwave Symposium.

기본 데모 2017-06-19

 
Video Clips from the "Four Ways to Boost Simulation Data Processing using Python" Webcast 
Watch these powerful video clips from the Keysight webcast, "Four Ways to Boost Simulation Data Processing using Python".

기본 데모 2017-06-12

 
Electrothermal Simulation using the Wolfspeed ADS PDK  
This is a short demonstration of how the Wolfspeed ADS PDK is configured to work with the ADS electrothermal simulator to co-simulate electrical and thermal performance. This allows designers to quickly understand the impact of thermal effects on their circuit designs, and account for those effects during the design process.

기본 데모 2017-06-02

 
Keysight 5G Trial System Design and Validation Solution Demo 
This video demonstrates Verizon’s early 5G trial system modeling connected to the latest 3GPP TR 38.900 mmWave channel model. These specifications facilitate early 5G trial system deployments and provide the wireless industry with the ability to test and validate key 5G technical components.

기본 데모 2016-12-19

 
키사이트 Genesys로 간편해진 합성  
키사이트 Genesys로 간편해진 합성 짧은 자습서 동영상으로 다양한 토폴로지와 여러 다양한 RF 회로를 빠르게 설계하는 방법을 알아보십시오. 이 단계별 자습서는 자동 RF 회로 및 시스템 합성 툴을 이용해 몇 시간씩 걸리던 일상적인 설계 작업을 몇 분 내에 완료할 수 있도록 해주는 단계들을 차례차례 설명합니다.

기본 데모 2016-12-01

 
Transform 5G Concepts into “This Changes Everything” Reality  
Evolve existing technologies. Invent new ones. Go from 5G waveform concept to “this changes everything" reality – while saving time, money and silicon. It starts with Keysight’s testbed for 5G waveform generation and analysis.

기본 데모 2016-10-19

 
The High-Frequency, High Speed Design Revolution: Why Your Design & Test Flow Will Soon Be Obsolete 
In this keynote from EDI CON USA 2016, Todd Cutler, vice president and general manager of Keysight Design & Test Software, discusses these trends and explains how, when coupled with market pressures, they are driving a revolution in the design and measurement industry.

기본 데모 2016-10-11

 
Unlocking Millimeter Wave Insights 
It is easy to underestimate the challenges at millimeter-wave frequencies, and this amplifies the importance of integrated tools for design, simulation, measurement, and analysis. Learn more about how Keysight is taking the mystique out of millimeter waves and unlocking new insights.

기본 데모 2016-09-30

 
Getting Started with ADS 
In this short video, you will learn how to navigate through the ADS environment to create a new workspace, build a new schematic, and run a simulation.

기본 데모 2016-09-11

 
How to Design Custom RF, Microwave and Analog Filters 
This video shows a custom filter design technique based on Direct or Exact Synthesis in which the filter response is first shaped and customized to meet specifications before a suitable topology is extracted and transformed for the most economical realization.

사용방법 동영상 2016-09-01

 
Introducing SystemVue 2016 
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

기본 데모 2016-06-27

 
How to Eliminate Layout Induced Oscillations 
This video describes how to predict and ultimately eliminate layout induced oscillation using electromagnetic analysis.

사용방법 동영상 2016-06-14

 
Harmonic Balance Simulation in Advanced Design System 
This video tutorial describes the set up and running of the harmonic balance simulator.

기본 데모 2016-06-13

 
IMS-MTT 2016 from Keysight EEsof EDA 
Highlights from Keysight EEsof EDA on the show floor at IMS-MTT 2016 in San Francisco, CA on May 22-26, 2016.

기본 데모 2016-06-05

 
전력 무결성을 위한 설계 방법: VRM 선택  
이 동영상은 전압 모드 VRM과 VRM 에러 앰프에 대한 션트 보상을 피해야 하는 이유에 대해 설명합니다. 에러 앰프에 대한 직렬 보상을 통한 전류 모드 VRM의 개선된 성능은 시뮬레이션과 측정을 통해 분명하게 시연됩니다.

사용방법 동영상 2016-05-05

 
Genesys Overview 
Genesys continues to offer the industry’s most powerful RF circuit and system synthesis capabilities in an affordable, accurate and easy-to-use simulation software that you’ve come to love. Keysight Sys-Parameters provide breakthrough convenience in using component datasheet parameters such as amplifier P1dB, IP3, gain and noise figure over frequency, temperature and bias for simulation without the need to create custom files and equations.

기본 데모 2016-02-11

 
유튜브의 ADS 동영상  
유튜브 키사이트 EEsof EDA 채널의 ADS(Advanced Design System) 동영상 라이브러리 재생 목록

기본 데모 2016-01-28

 
How to Understand 5G: Beamforming 
This video provides guidance for understanding what types of multi-antenna system architecture are being researched for the next generation standard. The examples with end-to-end link level simulation demonstrate key technical issues of different multi-antenna beamforming system design under mmWave channel environments.

사용방법 동영상 2015-11-23

 
Discovering Genesys 
A collection of Keysight EEsof EDA Genesys video demonstrations and tutorials

기본 데모 2015-08-27

 
How to Design DC-to-DC Converters 
This video introduces basic DC-to-DC converter operation, explains why voltage spikes occur in these circuits, and shows the importance of modeling PC board layout effects. There is an example in which current visualization is used to see potential problem areas in the PC board. The layout is then modified to improve performance.

사용방법 동영상 2015-08-24

 
Active Analog Filter Synthesis 
Learn how to quickly design active analog filters with op-amps from a complete selection of response shapes such as Chebyshev, Butterworth, Bessel Cauer or user-defined G-value tables. Select from all popular topologies such as biquad, elliptic, single or multiple feedback for fast realization with active filter synthesis. Includes singly terminated topologies for diplexer and multiplexer designs.

기본 데모 2015-08-15

 
Splitter, Coupler, Balun and Attenuation Synthesis 
Learn about RF/microwave signal control using splitters, combiners, couplers, baluns and attenuators. Then quickly design from 27 different popular topologies such as Wilkinson splitter, Lange Coupler and 90 degree branch line including generation of their distributed layouts on microstrips using signal control synthesis.

기본 데모 2015-08-15

 

1 2 3 4 5 다음