Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Application Information About Specific Components & Devices

Refine the List

remove all refinements

By Industry/Technology

By Type of Content

By Product Category

201-225 of 238

Sort:
Simplified Motor Spin-up Analysis (AN 1200-1) 
This Application Brief offers the Keysight 53310A Modulation Domain Analyzer as a solution to the problem of characterizing a motor's performance without the need for external controller.

Application Note 2000-08-01

Direct Characterization of Motion Control Systems (AN 1200-2) 
This Application Brief is one of a series. It demonstrates how the Keysight 53310A makes it easy to capture and view velocity profiles, without the need for an external controller.

Application Note 2000-08-01

Network Analysis - Filter And Amplifier Measurement Examples (AN 1287-4) 
The network analyzer is used for a variety of device and component characterization tasks in both laboratory and production environments.

Application Note 2000-08-01

Fundamentals of Modal Testing (AN 243-3) 
This modal test 56 page Application Note provides an verview of structural dynamics theory, the measurement process for acquiring frequency response data, parameter estimation (curve fitting), and the analytical techniques of structural analysis and their relation to experimental testing (such...

Application Note 2000-05-01

Testing CDMA Base Station Amplifiers (AN 1307) 
The objective of this Application Note is to cover the basic measurement fundamentals of characterizing the linear and non-linear behavior of CDMA power amplifiers.

Application Note 2000-05-01

Bearing Runout Measurements (AN 243-7) 
This Application Note introduces the challenge of making runout measurements in disk drives, which is a critical step in increasing storage capacity. It explains the test setup required and shows measurements of repeatable and non-repeatable runout, synchronous and asynchronous runout, and...

Application Note 2000-05-01

Improving Network Analyzer Measurements of Frequency-translating Devices (1287-7) – Application Note 
This Application Note explores current test equipment solutions and techniques that can be used to accurately characterize and test frequency-translating devices.

Application Note 2000-03-01

Keysight TestJet Technology White Paper 
This paper describes the Keysight TestJet technique, which makes use of a property of most digital ICs in use in the mid-1990s: the lead frame.

Application Note 2000-01-01

 
Low Cost Mixer for the 10.7 to 12.8 GHz Direct Broadcast Satellite Market (AN 1136) 
This Application Note is for information only. Keysight no longer sells or supports these products.

Application Note 1999-11-01

PDF PDF 54 KB
A Low Cost, Surface Mount X-Band Mixer (AN 1052) 
This Application Note is for information only. Keysight no longer sells or supports these products.

Application Note 1999-11-01

PDF PDF 35 KB
Printed Circuit Board Split-Pad Test Method and Design 
This application note describes the split-pad concept for use with a bed of nails style test fixture.

Application Note 1999-06-01

PDF PDF 50 KB
Test Strategy for Complex Printed Circuit Board Assemblies 
This paper proposes a new test strategy for complex boards since the trend in Printed Circuit Board Assembly (PCBA) technology is towards higher complexity.

Application Note 1999-02-22

PDF PDF 195 KB
Discreet Analog Device Testing 
The Keysight 3070 series has quite a few built in features to make developing board tests easier, while protecting the operator, the board under test, and the 3070 itself from harm.

Application Note 1998-10-29

PDF PDF 26 KB
Boundary-Scan Technology, Justification, and Test Implementation for Designers 
This paper provides practical insight for designers on the merits, design, and test implementation of Boundary-Scan Technology.

Application Note 1998-05-27

PDF PDF 29 KB
Boundary Scan Ground Bounce Suppression 
Boundary-Scan circuitry, while in the process of testing interconnections, can set up and excite current surges on a board. This in turn can cause "ground bounce".

Application Note 1998-04-24

PDF PDF 14 KB
Fixture Interface Pin (MINT Pin) Maintenance 
Fixture Interface Pins (MINT Pins) used in production testing will eventually get dirty enough to cause contact problems.

Application Note 1998-03-01

PDF PDF 20 KB
Effective Machinery Measurements Using Dynamic Signal Analyzers (AN 243-1) 
This Application Note outlines the benefits of vibration analysis and provides basic information on making machinery measurements. It explains how vibration is converted to electrical signals and how the frequency domain helps users identify the comp. of signal. It also identifies the vibration...

Application Note 1997-12-01

PDF PDF 1.40 MB
3070 Increasing Throughput 
There are decisions one can make that causes a Keysight 3070 test program to be slower or faster than what Test Consultant generates automatically. This paper offers many tips about how to optimize your system's performance.

Application Note 1997-03-03

PDF PDF 41 KB
How To Float, or Series, Keysight 3070 DUT Supplies 
The Keysight 3070 development software does an amazing job of calculating the wiring needed to build fixtures. Even so there are occasionally cases which require wiring that the standard Keysight 3070 software can not handle.

Application Note 1997-01-23

PDF PDF 34 KB
Selective Retrieval for Keysight 3070 Board Test Systems with UNIX Controllers 
Most users are very diligent about backing-up their systems in the event of a catastrophic disk failure. Typically, you use SAM to set-up periodic automated backups or create a "crontab" entry to do this.

Application Note 1996-07-01

 
Complete Analysis of Erbium-Doped Fiber Amplifiers 
This Technical Paper discusses methods and instruments for measuring EDFAs with respect to gain and noise figure, both in static and dynamic form, polarization dependence, polarization mode dispersion, WDM characteristics and more. The influence of the spectral width of the laser source on the...

Application Note 1996-03-01

PDF PDF 142 KB
Using Pop-up Windows 
There are occasions where the use of a pop-up window would be advantageous while testing boards on the Keysight 3070. This article is meant to highlight one method that can be used to obtain that end.

Application Note 1996-01-01

PDF PDF 18 KB
Electronic Heater Valves Testing (AN 1270-4) 
Production testing of heater/air conditioning system valves is performed on high speed HP automatic test systems with minimum operator interface. This Application Note describes a typical HP VXI system configuration for testing automotive heater/air-conditioning system valves.

Application Note 1995-06-01

PDF PDF 39 KB
Essential Testability Guidelines for Current Technology 
This paper addresses essential testability considerations, both electrical and mechanical, and focuses on new requirements of current technologies.

Application Note 1993-04-22

PDF PDF 55 KB
Fundamentals of the z-Domain and Mixed Analog/Digital Measurements (AN 243-4) 
This Application Note is for information only. Keysight no longer sells or supports these products.

Application Note 1989-08-01

PDF PDF 1.13 MB

Previous 1 2 3 4 5 6 7 8 9 10 Next