Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Basics & Measurement Fundamentals

Refine the List

remove all refinements

By Industry/Technology

By Type of Content

By Product Category

151-175 of 272

Sort:
Boundary Scan Helps EMS Companies Cut Test Costs and Increase Revenues 
Electronics Manufacturing Services (EMS) providers can utilize boundary-scan to reduce test cost expenses and also generate additional revenue opportunities.

Application Note 2003-03-01

PDF PDF 242 KB
PLR and 5DX Customized Defect Names Implementation 
You can use customized defect names on both the 5DX and on the PLR. This is particularly valuable when you want to display defect names in a local language.

Application Note 2003-03-01

 
Using Boundary Scan to Link Design and Manufacturing Test 
By leveraging boundary-scan tests generated in Design and re-using them at Manufacturing Test, manufacturers can produce long-term benefits in terms of lower costs, greater efficiencies and higher quality products.

Application Note 2003-03-01

PDF PDF 502 KB
What to Consider When Selecting the Optimal Test Strategy 
This paper addresses several issues for selecting the optimal inspection strategy, presenting data from many studies that Keysight has performed in the quest to find the optimal test / inspection strategy.

Application Note 2003-03-01

PDF PDF 175 KB
Jitter Analysis Techniques for High Data Rates (AN 1432) - Application Note 
This new application note describes the basic jitter measurements and the specific measurement techniques used in SONet/SDH/OTN and Gigabit Ethernet applications.

Application Note 2003-02-03

Ground Bounce Basics and Best Practices 
This article offers a description of the physical properties that result in ground bounce during board test.

Application Note 2003-01-28

PDF PDF 138 KB
System Issues in Boundary-Scan Board Test 
While Boundary-Scan is a powerful test tool, test engineers are finding out that yesterday's DFT rules and test approaches may actually be detrimental to successfully testing systems on a board.

Application Note 2003-01-28

PDF PDF 37 KB
New Features in Version 5.0 Software for 3070 
Typically, when Keysight's Manufacturing Test Division introduces a new software revision for its flagship 3070 In-Circuit Tester, it only communicates with customers about the major new features.

Application Note 2003-01-28

PDF PDF 84 KB
Design for Testability - Test for Designability 
This paper addresses testability considerations, both physical and logical, and focuses on both the new constraints and the new freedoms of modern manufacturing test in the ever-changing challenge.

Application Note 2003-01-28

PDF PDF 852 KB
Keysight 3070 Now Powered by Industrial PC Controllers 
The Keysight 3070 is now controlled by PCs similar to others used in your production and office environment lowering system administration and learning costs.

Application Note 2003-01-23

PDF PDF 207 KB
Connecting a UPS to a 3070 Controller 
This paper describes how to connect a UPS to the 3070 testhead controller. It uses the Advanced Power Conversion Smart-UPS with PowerChute Plus software.

Application Note 2003-01-07

PDF PDF 87 KB
A New Process for Measuring and Displaying Board Test Coverage 
Written by Kenneth P. Parker, Keysight Technologies. First presented at Apex 2003, Anaheim, California.

Application Note 2003-01-01

PDF PDF 116 KB
When to Use AOI, When to Use AXI, and When to Use Both 
by Stig Oresjo, senior test strategy consultant at Keysight Technologies.

Application Note 2002-12-01

PDF PDF 70 KB
An Introduction to Multiport and Balanced Device Measurements (AN 1373-1) 
The increase in integration in the wireless communications and electronics industries and the need to decrease size, cost, weight, and power consumption is driving design engineers to replace discrete components with more complex modules.

Application Note 2002-11-11

Preparing a .cc File for Export to Test Link 
This procedure describes the process of converting ECAD data into a form that can be used by Test Link.

Application Note 2002-10-16

PDF PDF 70 KB
Comparison of Mixer Characterization using New Vector Characterization Techniques – White Paper 
This paper presents a novel method for characterizing RF mixers, yielding magnitude, phase, and group delay response of the conversion loss, as well as the input match and output match.

Application Note 2002-10-04

UNIX vs. Windows Differences for 3070 Users 
This documentation serves as a PC transition guide to help existing 3070 customers migrate from the Unix platform to the PC platform.

Application Note 2002-09-19

 
Fundamentals of Signal Analysis Series (AN 1405-2) 
This application note is a primerfor those who are unfamiliar with the class of analyzers we call dynamic signal analyzers. These instruments are particularly appropriate for the analysis of signals in the range of a few millihertz to about a hundred kilohertz.

Application Note 2002-08-06

Windows & Unix Feature Comparison 
The Windows & Unix 3070 Feature Comparison document provides a detailed listing of features translated to the Windows based 3070 from the Unix based 3070.

Application Note 2002-07-31

PDF PDF 71 KB
3070 In System Programming (ISP) Family 
On Board Programming, Bottom Line Benefits

Application Note 2002-07-25

PDF PDF 200 KB
Remote Network Connections Creation for the Operator Logon 
Operator logon on the Keysight 5DX Series II System is limited, in that it does not allow Operator to make network connections that are required for sending images and res files to the PLR workstation.

Application Note 2002-06-30

 
Using NDFCOL.EXE, the NDF "Line Up the Columns" Utility 
NDFCOL.EXE is a handy little utility that will form neat columns of data in NDF files.

Application Note 2002-06-06

 
Obtaining a Listing of Applications on Series II Systems 
There is currently no easy way to obtain a list of all resident applications on a 5DX System or TDW. It is difficult to match panel name with hash name and see when the application was last updated.

Application Note 2002-06-01

 
Fundamentals of Signal Analysis Series (AN 1405-1) 
This Application Note is a primer for those who are unfamiliar with the advantages of analysis in the frequency and modal domains.

Application Note 2002-05-24

Sampling on the Keysight 5DX 
Sampling Mode allows test coverage to be optimized with line speed. This document explore the setup procedure for the Keysight 5DX for sampling.

Application Note 2002-05-08

 

Previous 1 2 3 4 5 6 7 8 9 10 ... Next