您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

MIMO 測試

MIMO(多路輸入/多路輸出)是一項具有挑戰性的天線技術,可提高頻譜效率(位元/秒/Hz)、信號品質和細胞覆蓋率。MIMO 可用於多種技術,包括 LTE-Advanced、WLAN 和現在正進行密集研究的新型 5G 技術。這項複雜技術,同時也是不斷演進的標準,MIMO 變成了開發過程中的瓶頸,而且需要使用特定的量測套件。是德科技解決方案旨在提供更深入的洞察力,並隨著標準演進而推動開發。當您進行設計和測試時,是德科技解決方案讓您能在新型和現有技術上進行創新,並可協助工程師落實其概念與創意。

MIMO Test Insights

觀看YouTube影片 

1-8 / 8

排序:
Introduction of LTE-Advanced Signal Generation and Analysis at Mobile World Congress March 2011 
Keysight’s European Marketing Manager, Renaud Duverne, introduces new capabilities capabilities such as carrier aggregation and answers questions about LTE-A early adoption, reducing the cost of test, transformative technologies and the challenges of growing video traffic.

基本展示 2011-03-14

 
Demonstration of analysis of un-impaired and impaired WiMAX(TM) MIMO signal  
This video contains an analysis of a 2x2 WiMAX MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an un-impaired signal and signal impaired by pedestrian fading are examined.

基本展示 2011-03-02

 
Option B7Z IEEE 802.11n MIMO Modulation Analysis 89600 Vector Signal 
This demonstration guide provides step by step instructions for making 802.11n MIMO measurements using the 89600 VSA software.

基本展示 2011-02-25

Demonstration of analysis of an un-impaired MIMO WiFi signal 
This video demonstrates how Keysight’s N7100 Multichannel signal analysis platform can identify and troubleshoot problems in a WiFi signal.

基本展示 2011-02-22

 
Demonstration of analysis of un-impaired and impaired LTE MIMO signal 
This video contains an analysis of a 2x2 LTE MIMO signals using the N7100 Multi-channel Signal Analysis Platform and the 89600 Vector Analysis Software. Both an unimpaired signal and signal impaired by static fading are examined.

基本展示 2011-02-22

 
N7100 Multi-channel Signal Analysis support of MIMO development 
The N7100 Multi-channel analysis platform helps solve difficult problems in MIMO development. The video is an overview of the many measurement and analysis capabilities of the N7100.

基本展示 2011-02-22

 
LTE MIMO Composite EVM  
This is a demonstration of a 2x2 LTE MIMO system configuration where the Keysight 89600 VSA software and Keysight N9020A MXA signal analyzers are used to make an LTE MIMO composite EVM measurement on signals from the Keysight N5182A MXG signal generators.

基本展示 2011-01-12

 
MIMO Signal Analysis Videos 
Measurement demonstrations on a WLAN MIMO device

基本展示 2008-09-29