这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

是德科技蜂窝测试技术

是德科技公司是全球领先的测试与测量公司,可以提供全方位的设计、测试和管理解决方案。这些解决方案覆盖整个蜂窝技术领域――从传统1G系统到3G系统(例如HSPA),再到3GPP 长期演进技术(LTE)和1xEV-DO。是德的产品适用于从早期设计与开发、批量制造到网络部署和服务保障的全过程。推动蜂窝技术的创新与发展,是德为您披荆斩棘!

 

#5G #LTE-Advanced (LTE-A) #LTE测试 #毫微微蜂窝基站测试 #包络跟踪功率放大器 #HSPA和HSPA+ #W-CDMA #TD-SCDMA #GSM、GPRS、EGPRS和EDGE/Evo #1xEV-DO #cdma2000®/CDMA #多标准无线(MSR)#全球导航卫星系统(GNSS)和辅助 GNSS(A-GNSS)设计与测试解决方案 #TDMA

查看相关视频(优酷) 

1-2 / 2

排序:
Measuring the Burst Time-Gated Power Signal of Wireless Technologies Using Keysight Power Sensors 
Measuring pulse, burst, or modulated signals for wireless technologies such as TDMA, GSM, WLAN, WiMAX, and LTE is very important because it is part of functionality testing and power amplifier module verification during the manufacturing process.

应用说明 2013-07-08

U2000 Series USB Power Sensor GSM Timeslot Burst Power Measurement - Application Note 
The demo guide explains the simplest steps to measure burst, modulated and pulse signals using the cost effective U2000 Series USB power sensor.

应用说明 2009-10-06

PDF PDF 545 KB