Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Aerospace & Defense

Focus where it counts

Missions evolve but one thing stays the same: the need to protect those who go in harm's way. Success depends on a changing mix of people and technology. As technology becomes more complex, assuring readiness gets tougher.

Keysight is a source of assurance that your mission will succeed. Through our expertise in measurement science and test processes, we give you more time for the bigger issues: fulfilling today's mission and managing the transition to what comes next. By helping you build greater assurance in system readiness, Keysight frees you to focus where it counts most.

1-16 sur 16

Tri:
Introducing SystemVue 2016 
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

Démonstration de base 2016-06-27

 
NewSpace and Traditional Space panel session– recorded at the NewSpace 2015 conference 
Streamed live on July 16, 2015, this video is a panel discussion of important key players in the NewSpace arena.

Démonstration de base 2016-02-02

 
Precision Validation of Radar System Performance in the Field Using FieldFox 

Démonstration de base 2014-03-21

 
Realistic Ultra Wideband Radar Signal - Demo 
Testing of radar systems can be extremely time-consuming and expensive. Radar transceivers must be designed and tested with realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators.

Démonstration de base 2013-11-25

 
EVM measurement with the new M8190A Arbitrary Waveform Generator - video  
To meet the high demands of aerospace/ defense application tests, it is indispensable to simulate real-life scenarios with precision arbitrary waveforms. In a test setup with a high error vector magnitude (EVM), problems within your device under test may not be discovered. With signals close to reality, the Keysight M8190A is the perfect solution.

Démonstration de base 2012-08-20

 
Reconfigurable Radar Design: Debug and Validation - video 
This video demonstrates how to debug and validate reconfigurable radar design with Keysight test and measurement instruments and software.

Démonstration de base 2012-07-30

 
OFDMA Concepts Demonstration - channel training sequence - video 
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

Démonstration de base 2012-06-11

WMF WMF 20.57 MB
Microwave Switch Repeatability Demonstration - video 
This video compares the repeatability performance of a Keysight microwave switch with a competitor’s offering. Performance is compared by measuring the insertion loss across a frequency range, then comparing the relative difference of each insertion loss measurement.

Démonstration de base 2012-06-11

WMF WMF 17.78 MB
Interference Mitigation Through the Use of Wideband Signal Recording and Analysis - video  
This video describes the process to find and analyze the cause of a radio signal that is interfering with a wireless LAN transmitter. This requires the continuous capture of wireless spectrum, tools to search and find possible interferers as well as tools to determine how an interferer may affect the LAN signal.

Démonstration de base 2012-06-11

WMF WMF 33.25 MB
Reproducing DC Power Transients, Using an N6705B DC Power Analyzer to Create Transients - video 
DC power transients can easily be reproduced with N6705B DC Power Analyzer. Power transients can be used to test a DUT resilience to a change in voltage. Two examples are provided an automobile's voltage during engine turn-on and a PS interrupt specified in the DO-160F avionics test manual. Transients can also occur when the load on a PS changes.

Démonstration de base 2012-05-10

 
OFDMA Concepts Demonstration - channel training sequence - video  
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

Démonstration de base 2012-05-10

 
Measuring Performance of Wide Bandwidth Radar Transmitters 
Short videos on measuring performance of wide bandwidth radar transmitters.

Démonstration de base 2011-04-21

 
Self-diagnosing Switch Matrix 
Self-diagnosing Switch Matrix

Démonstration de base 2011-02-16

 
Signal Studio for Global Navigation Satellite Systems N7609B Video Demonstrations 
View this series of three videos which will provide an introduction to the N7609B Signal Studio for Global Navigation Satellite Systems (GNSS) software and demonstrates some of the key features of the software.

Démonstration de base 2010-03-30

 
P-Series Power Meter Radar Video Demonstrations 

Démonstration de base 2009-04-01

 
E3238S / 35688E Product Tour DVD 

Démonstration de base 2006-11-28

PDF PDF 185 Bytes