Contact an Expert

Network Analyzer for Crystal Devices

The E5100A high-speed network analyzer is an excellent solution for electronic component manufacturers, especially resonator, filter manufacturers and crystal devices, who require extra-high throughput. The E5100A improves production line productivity with its fast measurement speed (fastest sweep speed is 0.04 ms/point), fast waveform analysis commands, and high-speed processor. The E5100A's low-noise performance and fine selection IFBW provide high quality measurements with lower fluctuations.

Discontinuance Notice: Some options and upgrade kit for the E5100A network analyzers were discontinued as of May 1, 2006. For more details, click here.

Refine the List

By Type of Content

By Product Category

1-24 of 24

Network Analyzer - Selection Guide
Provides an overview of Keysight’s network analyzer families, recommended solutions for various applications, related network analyzer products, and a comparison of specifications and features.

Selection Guide 2015-08-19

Understanding the Fundamental Principles of Vector Network Analysis - Application Note 1287-1
This application note explores the fundamental principles of vector network analysis. The discussion includes the common parameters (S-parameters). RF fundamentals such as transmission lines and the Smith chart will also be reviewed.

Application Note 2015-05-15

Improved Throughput in Network Analyzer Applications (AN 1287-5)
This Application Note explores a variety of throughput issues and how they might affect different applications. It suggests ways to improve network analyzer performance for better throughput in specific situations, and how to get an accurate picture of how an analyzer's performance might impact...

Application Note 2010-03-15

Printer Compatibility
This page explains the printer support policy and the latest printer compatibility updates.

User Manual 2009-02-10

Network Analyzer Selection Guide (For Reference Only - Includes Discontinued Products)
This document does not contain the most up-to-date information. The document is available for reference only, for customers using legacy network analyzers. Current document:

Selection Guide 2009-02-03

E5100A Security Features
This document describes instrument security features and the steps to declassify an instrument through memory sanitization or removal.

Reference Guide 2008-02-01

E5100A Technical Overview
The E5100A is a 10 kHz to 300 MHz network analyzer, best fitted for production lines of electronic component manufacturers, especially crystal and ceramic resonators or crystal and ceramic filter manufacturers

Technical Overview 2006-07-13

Crystal Resonator Measuring Functions of E5100A Network Analyzer (PN E5100A-2)
This Product Note describes about crystal resonator measurement using network analyzer, E5100A.

Application Note 2006-07-13

E5100A Data Sheet
These specifications are the performance standards of limits against which the instrument is tested when shipped from the factory. The E5100A meets the specifications listed in this section.

Data Sheet 2006-07-13

Keysight E5100A Network Analyzer Latest Information for Manuals
The following changes should be followed to adapt the existing manuals to the newer instruments.

Operation Manual 2006-05-01

E5100A/E5100B User's Guide
This manual describes the method to set up and basic operations of E5100A/B in simple steps.

User Manual 2003-05-01

E5100A Network Analyzer Option 218/318/618/823 Manual Supplement

Operation Manual 2003-05-01

E5100A/E5100B Function Reference
This manual describes all function accessed from the front panel keys and softkeys.

Reference Guide 2003-05-01

Network Analysis Basics - Applying Error Correction To Network Analyzer Measurements (AN 1287-3)
Only perfect test equipment would not need correction. Imperfections exist in even the finest test equipment and cause less than ideal measurement results.

Application Note 2002-03-27

Network Analysis Basics - 10 Hints for Making Better Network Analyzer Measurements (AN 1291-1B)
This Application Note contains hints to help you understand and improve your use of network analyzers, and a summary of network analyzers and their capabilities.

Application Note 2001-09-17

E5100A/E5100B Programming Manual
This manual describes how to write and use BASIC program to control the analyzer and provides a summary of all available GPIB commands.

Programming and Syntax Guide 2001-07-01

E5100A/E5100B HP Instrument BASIC Users Handbook Supplement
This manual help you to became familiar with the operation of the analyzer and the BASIC programming language.

User Manual 2001-07-01

Exploring the Architectures of Network Analyzers (1287-2) – Application Note
This Application Note explains that Network analyzers have become one of the most important tools for characterizing the performance of high-frequency components and devices.

Application Note 2000-12-06

Instrument Basic Users Handbook Version 2.0
This manual describes how to use IBASIC program.

User Manual 2000-12-01

PDF PDF 33.46 MB
Network Analysis - Filter And Amplifier Measurement Examples (AN 1287-4)
The network analyzer is used for a variety of device and component characterization tasks in both laboratory and production environments.

Application Note 2000-08-01

E5100U Option 024 Upgrade Kit Installation Manual

Installation Manual 2000-07-01

E5100A Network Analyzer Manual Supplement for Option 510

Operation Manual 2000-07-01

E5100A Network Analyzer Manual Supplement for Option 509

Operation Manual 2000-07-01

Fundamentals of Quartz Oscillators (AN 200-2)
The purpose of this classic Application Note is to provide a background on the crystal reference element and its impact in an oscillator circuit. It then explains the effects of the oscillator on the accuracy of a frequency measurement and frequency generation.

Application Note 1997-05-01